:TDR:DEEMbed:DUT:PORT:TPORt
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:DEEMbed:DUTN:PORTM:TPORt {NCONnected | {PORTM}
Where N indicates one of 16 possible DUT setups. For example, :DUT4.
Where M indicates one of 16 possible DUT ports. For example, :PORT3.
Description
Specifies with fixture component port that will function as the test port for the selected DUT port. Use the :TDR:DEEMbed:DUT:PORT:DPORT command to select which fixture component port is connected the DUT. The following table shows examples of how the commands are used to configure a fixture component setup. Refer to the :TDR:DEEMbed:DUT:ENABle command for more information. The query form of the command returns {NCON | {PORT{1:16}}.
| Setup | Command Sequence | Item |
|---|---|---|
1-Port Single Ended![]() |
:TDR:DEEMbed:DUT1:PORT1:FIXTure FCOMA :TDR:DEEMbed:DUT1:PORT1:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT1:DPORt PORT2 |
1 2 3 |
1-Port Differential![]() |
:TDR:DEEMbed:DUT1:PORT1:FIXTure FCOMA :TDR:DEEMbed:DUT1:PORT1:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT1:DPORt PORT2 :TDR:DEEMbed:DUT1:PORT2:FIXTure FCOMB :TDR:DEEMbed:DUT1:PORT2:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT2:DPORt PORT2 |
1 2 3 4 5 6 |
2-Port Single Ended![]() |
:TDR:DEEMbed:DUT1:PORT1:FIXTure FCOMA :TDR:DEEMbed:DUT1:PORT1:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT1:DPORt PORT2 :TDR:DEEMbed:DUT1:PORT2:FIXTure FCOMB :TDR:DEEMbed:DUT1:PORT2:TPORt PORT2 :TDR:DEEMbed:DUT1:PORT2:DPORt PORT1 |
1 2 3 4 5 6 |
2-Port Differential![]() |
:TDR:DEEMbed:DUT1:PORT1:FIXTure FCOMA :TDR:DEEMbed:DUT1:PORT1:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT1:DPORt PORT2 :TDR:DEEMbed:DUT1:PORT3:FIXTure FCOMA :TDR:DEEMbed:DUT1:PORT3:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT3:DPORt PORT2 :TDR:DEEMbed:DUT1:PORT2:FIXTure FCOMB :TDR:DEEMbed:DUT1:PORT2:TPORt PORT2 :TDR:DEEMbed:DUT1:PORT2:DPORt PORT1 :TDR:DEEMbed:DUT1:PORT4:FIXTure FCOMB :TDR:DEEMbed:DUT1:PORT4:TPORt PORT2 :TDR:DEEMbed:DUT1:PORT4:DPORt PORT1 |
1 2 3 4 5 6 7 8 9 10 11 12 |
4-Port Single Ended![]() |
:TDR:DEEMbed:DUT1:PORT1:FIXTure FCOMA :TDR:DEEMbed:DUT1:PORT1:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT1:DPORt PORT2 :TDR:DEEMbed:DUT1:PORT3:FIXTure FCOMA :TDR:DEEMbed:DUT1:PORT3:TPORt PORT1 :TDR:DEEMbed:DUT1:PORT3:DPORt PORT2 :TDR:DEEMbed:DUT1:PORT2:FIXTure FCOMB :TDR:DEEMbed:DUT1:PORT2:TPORt PORT2 :TDR:DEEMbed:DUT1:PORT2:DPORt PORT1 :TDR:DEEMbed:DUT1:PORT4:FIXTure FCOMB :TDR:DEEMbed:DUT1:PORT4:TPORt PORT2 :TDR:DEEMbed:DUT1:PORT4:DPORt PORT1 |
1 2 3 4 5 6 7 8 9 10 11 12 |
Requires FlexDCA revision A.05.30 and above.