:TDR:DEEMbed:FCOMponent:STATus?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:DEEMbed:FCOMponentF:STATus?
Where F identifies a specific fixture component. There can be up to sixteen fixture components identified by letters A through P. For example, FCOMA.
Query Response
{CORR | INV | QUES}
- CORR
- The fixture component is defined.
- INV
- The fixture component is invalid.
Description
Queries the status of a Fixture Component for Fixture De-Embedding Setups (:TDR:DEEMbed:DUT:ENABle). Fixture components are created using the :TDR:DEEMbed:FCOMponent:LOAD command. Use the STATus:REASon? child query to determine the reason for an invalid status.
Requires FlexDCA revision A.05.30 and above.