:TDR:DEEMbed:FCOMponent:NOPorts?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:DEEMbed:FCOMponentF:NOPorts?
Where F identifies a specific fixture component. There can be up to sixteen fixture components identified by letters A through P. For example, FCOMA.
Description
Queries the number of ports in the selected Fixture Component. The number of ports in a fixture component is defined by the number of ports defined in the imported s-parameter file (:TDR:DEEMbed:FCOMponent:LOAD:FNAMe). For example, importing a four-port s-parameter file results in a four-port fixture component.
Requires FlexDCA revision A.05.30 and above.