:TDR:DEEMbed:FCOMponent:STATus:REASon?
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:TDR:DEEMbed:FCOMponentF:STATus:REASon?
Where F identifies a specific fixture component. There can be up to sixteen fixture components identified by letters A through P. For example, FCOMA.
Description
Returns a string that explains the reason for an invalid Fixture component. For example, if the fixture component does not exist the returned string would be "Please select a file.". If the setup is correct, a null string is returned. Use the parent :TDR:DEEMbed:FCOMponent:STATus? query, to return the status of a fixture component.
Requires FlexDCA revision A.05.30 and above.