:TDR:DEEMbed:FCOMponent:LOAD
Command Syntax
:TDR:DEEMbed:FCOMponentF:LOAD
Where F identifies a specific fixture component. There can be up to sixteen fixture components identified by letters A through P. For example, FCOMA.
Description
Creates the specified fixture component by loading an S-parameter file. The new fixture component is identified by a letter (A through P). To specify the file, use the :TDR:DEEMbed:FCOMponent:LOAD:FNAMe command. The number of ports that are defined in the imported s-parameter file determines the number of ports in the resulting fixture component. To delete an existing Fixture Component, use the :TDR:DEEMbed:FCOMponent:CLEar command.
To learn how to add fixture components to a Fixture De-Embedding Setups, refer to the :TDR:DEEMbed:DUT:ENABle command. To query the number of ports in an existing fixture component, use the :TDR:DEEMbed:FCOMponent:NOPorts query. To change the interpretation of the port location order on an existing fixture component, use the :TDR:DEEMbed:FCOMpnent:PORDer command. Use the :STATus child command to determine if the fixture component was created.
Requires FlexDCA revision A.05.30 and above.