:TDR:STIMulus:CHANnel:SKEW
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:TDR:STIMulus:CHANnel{1:8}{A|B|C|D}:SKEW <seconds>
Where {1:8}{A|B|C|D} identifies a channel. For example, 2A. For differential channels, the alpha portion of the identifier to select from is {A|C}. For example, 1A but not 1B.
Where the <seconds> argument is a double.
Query Syntax
:TDR:STIMulus:CHANnel{1:8}{A|B|C|D}:SKEW?
Description
Manually enters the TDR step skew for the specified channel. To automatically set the step skew, use the Step Deskew Wizard (:TDR:DESKew:STARt). To manually enter the software skew, use the :CHANnel:TDELay command.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TDR:STIMulus:CHANnel2A:SKEW 0.0E+0