:TRACe:OPERator
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Command Syntax
:TRACe{1:128}:OPERator {NONE | OHMS | VOLTs | PERCent | MAGNitude | PHASe | GDELay}
Where the {1:128} specifier identifies a trace.
Query Syntax
:TRACe{1:128}:OPERator?
Description
Specifies the type of graph in which to display a T-domain parameter trace or S-parameter trace. The following table shows the content window graph selected by each command argument. A T-domain parameter trace can be displayed in one of three content windows. An S-parameter trace can also be displayed in one of three content windows. To display the same parameter in all three graphs, define three separate traces. Use the :TRACe:PARameter command to assign the actual parameter to the trace.
| Command Argument |
Content Windows | |
|---|---|---|
| T-Domain Parameters | S-Parameters | |
| OHMS | Time-Ohms | |
| VOLTs | Time-Volts | |
| PERCent | Time-% | |
| MAGNitude | Freq-Mag | |
| PHASe | Phase | |
| GDELay | GrpDelay | |
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:OPERator OHMS