:TRACe:PARameter
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Command Syntax
:TRACe{1:128}::PARameter {NONE | <parameter>}
The <parameter> argument is the time-domain parameter or S-parameter name with an underscore (_) character between the numbers. For example, the argument for an S21 parameter is S2_1.
Where the {1:128} specifier identifies a trace.
Query Syntax
:TRACe{1:128}:PARameter?
Description
Assigns a T-domain parameter or S-parameter to the specified trace. Use the :TRACe:OPERator command to specify the graph in which to display the parameter. The query form of this command returns the parameter currently assigned to the specified trace. If a parameter has never been assigned to a trace, the query returns NONE.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:TRACe9:DUT DUT2 :TRACe9:PARameter S1_1 :TRACe9:OPERator VOLTs :TRACe9:COLor TCOLor3 :TRACe9:DISPlay ON