:TRACe:UNAMe
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Command Syntax
:TRACe{1:128}:UNAMe <string>
Where the {1:128} specifier identifies a trace.
Query Syntax
:TRACe{1:128}:UNAMe?
Description
Assigns a custom user name to a trace waveform. User names are helpful because they identify what a waveform represents rather than a T-domain parameter or S-parameter name. For example, you could assign user name "Gain of DUT 2" instead of T21. User names can be 25 characters or less and are displayed on the screen and on screen captures. To remove a custom user name, re-create it using an empty string.
Custom user names can by created for other waveforms using the following commands:
:CHANnel:UNAMe:CMODe:UNAMe:DIFF:UNAMe:EMEMory:UNAMe:FUNCtion:UNAMe:TDR:DUT:DIFFerential:NPORt:UNAMe:TDR:DUT:DIFFerential:PPORt:UNAMe:TDR:DUT:DIFFerential:SIGNal:UNAMe:WMEMory:UNAMe
This subsystem Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe4:UNAMe "Gain of DUT 2"