:TRACe:STATus?
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Query Syntax
:TRACe{1:128}:STATus?
Where the {1:128} specifier identifies a trace.
Query Response
{AVA | UNAV}
Description
Queries the availability of a trace for use. A trace becomes available (AVA) after it is defined and displayed. Available traces are not shown in the Signals Palette. An available trace's waveform may or may not be displayed. A trace is unavailable (UNAV) unless it has been defined using all of the following three commands:
:TRACe:DUTcommand.:TRACe:OPERatorcommand.:TRACe:PARametercommand.
A trace does not have to be displayed to be available.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:STATus?