:TRACe:XPOSition?
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Query Syntax
:TRACe{1:128}:XPOSition?
Where the {1:128} specifier identifies a trace.
Description
Queries the value at the center of the X-axis for the graph of the indicated T-domain parameter or S-parameter trace. Use the :TRACe:XSCale? command to query the scale of the horizontal axis. Query the value at the left side of the graph using the :TRACe:XLEFt? command. Query the value at the ride side of the graph using the :TRACe:XRIGht? command.
| Content Window Graphs | Y-Axis Units |
X-Axis Units |
|---|---|---|
| T-Domain Parameters | ||
| Time-Ohms | Ohms | Seconds |
| Time-Volts | Volts | |
| Time-% | Percent | |
| S-Parameters | ||
| Freq-Mag | Decibels | Hertz |
| Phase | Degrees | |
| GrpDelay | Seconds | |
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:XPOSition?