:TRACe:YBOTtom?
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Query Syntax
:TRACe{1:128}:YBOTtom?
Where the {1:128} specifier identifies a trace.
Description
Queries the Y-axis value at the bottom of the graph for the indicated T-domain parameter or S-parameter trace. Use the :TRACe:YUNits command to return the units-of-measurement. Use the :TRACe:OPERator command to return the type of graph and the :TRACe:PARameter command to return the actual T-domain parameter or S-parameter viewed.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:YBOTtom?