:TRACe:YUNits?
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Query Syntax
:TRACe{1:128}:YUNits?
Where the {1:128} specifier identifies a trace.
Query Response
{OHM | VOLT | PERC | DEGR | SEC | DEC}
Description
Queries the Y-axis units-of-measurement for the indicated T-domain parameter or S-parameter trace. The returned strings are described in the following table.
| Returned String |
Y-Axis Units |
Content Window Graphs | |
|---|---|---|---|
| T-Domain Parameters | S-Parameters | ||
| OHM | Ohms | Time-Ohms | |
| VOLT | Volts | Time-Volts | |
| PERC | Percent | Time-% | |
| DEC | Decibels | Freq-Mag | |
| DEGR | Degrees | Phase | |
| SEC | Seconds | GrpDelay | |
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:YUNits?