:TRACe:XUNits?
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Query Syntax
:TRACe{1:128}:XUNits?
Where the {1:128} specifier identifies a trace.
Query Response
{SEC | HERT}
Description
Queries the X-axis units-of-measurement for the indicated T-domain parameter or S-parameter trace. The units for T-domain parameters is seconds which is indicated with the returned SEC string. The units for S-parameters is Hertz which is indicated with the returned HERT string.
| Returned String |
X-Axis Units |
Content Window Graphs | |
|---|---|---|---|
| T-Domain Parameters | S-Parameters | ||
| SEC | Seconds | Time-Ohms | |
| Time-Volts | |||
| Time-% | |||
| HERT | Hertz | Freq-Mag | |
| Phase | |||
| GrpDelay | |||
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:XUNits?