:TRACe:YOFFset?
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Query Syntax
:TRACe{1:128}:YOFFset?
Where the {1:128} specifier identifies a trace.
Description
Queries the vertical offset value for the graph of the indicated T-domain parameter or S-parameter trace. This is the value at the center of the Y-axis scale. Use the :TRACe:YSCale command to set or query vertical scale. You can query the value at the top of the graph using the :TRACe:YTOP? command. You can query the value at the bottom of the graph using the :TRACe:YBOTtom? command.
| Content Window Graphs | Y-Axis Units |
X-Axis Units |
|---|---|---|
| T-Domain Parameters | ||
| Time-Ohms | Ohms | Seconds |
| Time-Volts | Volts | |
| Time-% | Percent | |
| S-Parameters | ||
| Freq-Mag | Decibels | Hertz |
| Phase | Degrees | |
| GrpDelay | Seconds | |
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:YOFFset?