:TRACe:XLEFt?
Instrument:
N1000A
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Query Syntax
:TRACe{1:128}:XLEFt?
Where the {1:128} specifier identifies a trace.
Description
Queries the X-axis value at the left edge of the graph for the indicated T-domain parameter or S-parameter trace. Use the :TRACe:XSCale? query to return the scale. Use the :TRACe:XUNits? command to return the units-of-measurement. Use the :TRACe:OPERator? command to return the type of graph and the :TRACe:PARameter? command to return the actual T-domain parameter or S-parameter viewed.
Requires FlexDCA revision A.04.00 and above.
Example Command
:TRACe2:XLEFt?