:WAVeform:YFORmat:WORD:ENCoding:HOLe?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:YFORmat:WORD:ENCoding:HOLe?
Description
Returns the data value 31,232 which is used to represent a waveform data point that has no sample data. To return the number of data points that contain holes, use the :WAVeform:YFORmat:POINts:HOLes? query. This condition applies to Y-format data (:WAVeform:YFORmat:WORD:YDATa).