:WAVeform:YFORmat:WORD:ENCoding:YORigin?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:YFORmat:WORD:ENCoding:YORigin?
Description
Returns the amplitude origin value used to scale the data points of Y-formatted 16-bit integer data(:WAVeform:YFORmat:WORD:YDATa?). The data values are raw analog-to-digital converter counts and must be converted to voltage units using the following waveform information:
Use the :WAVeform:YFORmat:WORD:ENCoding:YINCrement? query to return the Y origin value.