:WAVeform:YFORmat:WORD:ENCoding:CLOW?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:YFORmat:WORD:ENCoding:CLOW?
Description
Returns the data value 31,744 which is used to represent a waveform data point that is clipped low. This indicates a data point's amplitude that is too low to be displayed on the screen. Use the :SYSTem:AUToscale command to properly scale the waveform to the display. To return the number of data points that are clipped low, use the :WAVeform:YFORmat:POINts:CLIPped:LOW? query. This condition applies to Y-format data (:WAVeform:YFORmat:WORD:YDATa).