:WAVeform:YFORmat:WORD:ENCoding:CHIGh?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:YFORmat:WORD:ENCoding:CHIGh?
Description
Returns the data value 32,256 which is used to represent a waveform data point that is clipped high. This indicates a data point's amplitude that is too high to be displayed on the screen. Use the :SYSTem:AUToscale command to properly scale the waveform to the display. To return the number of data points that are clipped high, use the :WAVeform:YFORmat:POINts:CLIPped:HIGH? query. This condition applies to Y-format data (:WAVeform:YFORmat:WORD:YDATa).
For FlexDCA revisions below A.03.00, the longform of this query was CHIGT?. As of A.03.00, the query was changed to CHIGH?.