:WAVeform:YFORmat:POINts:HOLes?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:YFORmat:POINts:HOLes?
Description
Queries the number of points in the waveform's YFORmat data that have no sample data. If you are returning WORD formatted data, "hole" data points have the value 31232, as specified by the :WAVeform:YFORmat:WORD:ENCoding:HOLe? query. For all other formats, "hole" data points have the value NaN (9.91E+37). Use the :SYSTem:AUToscale command to properly scale the waveform to the display. Use :WAVeform:SOURce to select the source waveform.
Requires FlexDCA revision A.03.00 and above.