:WMEMory:XSCale
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory:XSCale <horizontal_scale>
<horizontal_scale> is a double.
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:XSCale?
Description
Sets the horizontal scale which is stored for the selected waveform memory. It may or may not be the same as FlexDCA's current setting. Multiply the horizontal scale by 10 to obtain the horizontal range. The default value is 100 ps.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.