:WMEMory:SRSYmbol
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:SRSYmbol
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Description
Realigns the timebase to use the earliest waveform memory pattern data as the reference symbol for the pattern. You can first select the reference symbol in the data using the :TIMebase:Find:Sequence and :TIMebase:FIND:NEXT commands as show here:
:TIMebase:FIND:SEQuence "1101" :TIMebase:FIND:NEXT
To automatically determine the reference symbol for the waveform memory pattern data and align the timebase with the reference symbol use the :TRIGger:PALign command.
This feature is only available in Scope mode.
Requires FlexDCA revision A.06.50 and above.