:WMEMory:YUNits?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Query Syntax
:WMEMory{1:8}:YUNits?
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Description
Queries the waveform memory's vertical units which is stored for the selected waveform memory.
| Unit | Returned Value |
|---|---|
| V | VOLT |
| V2 | VOLT2 |
| W | WATT |
| W2 | WATT2 |
| unknown | UNKN |