:WMEMory:YTOP?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Query Syntax
:WMEMory{1:8}:YTOP?
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Description
Queries the amplitude value stored in waveform memory that corresponds to the graticule's top edge. This is the value that existed when the source waveform was saved into memory or, if the data was loaded into memory from a file (:DISK:WAVeform:SAVE), it is the value that existed when the file was created. It may or may not be the same as FlexDCA's current setting.