Advanced Eye DJ (δ-δ)

Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8

The Advanced Eye DJ (σ-σ) measurement measures the DJ and can use an optional fixed RJ to perform jitter decomposition. When the measurement is selected, the Select Measurement Settings dialog appears with the Fix RJ field for entering an RJ Value that you have previously measured. This value of RJ is often measured using a shorter pattern. The Fix RJ and RJ Value fields can be configured from any of the advanced eye RJ, DJ, Jn, or TJ setup dialogs.

Changing the Fix RJ or RJ Value setting in any of the RJ, DJ, Jn, or TJ setup dialogs changes the setting in the remaining three dialogs.

Advanced eye leverages the DCA-X's ability to measure ultra-low levels of Random Jitter (RJ). This can be used to obtain fixed RJ values.

SCPI Command

:MEASure:EYE:DJ