NRZ Eye Measurements Toolbar

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ

Measurements on the Eye Mode toolbar support NRZ waveforms. The following three measurements also support PAM4, PAM6, and PAM8 waveforms: Average Power, Database Peak Hits, and OMA at Crossing. To perform measurements on PAM4, PAM6, and PAM8 waveforms, use the PAM toolbar.

NRZ Eye Measurements and Supported Waveforms
Measurement Waveform Types
NRZ PAM4 PAM6 PAM8
Average Power ● ● ● ●
Bit Rate ●
Crossing Percentage ●
Crossing Time ●
Database Peak Hits ● ● ● ●
Delta Time ●
Duty Cycle Distortion ●
Eye Amplitude ●
Eye Height ●
Eye Width ●
Extinction Ratio ●
Fall Time ●
Jitter ●
OMA at Crossing ● ● ● ●
One Level ●
Rise Time ●
Signal-to-Noise Ratio ●
TDEC ●
VECP ●
Zero Level ●