PAM Toolbar

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4

If the PAM-N Analysis software option is installed, you can make the PAM4 measurements that are shown on the toolbar. The PAM toolbar includes a link to the PAM setup dialog. Use the setting in the dialog to define measurement parameters for both Oscilloscope and Eye/Mask modes. The Linearity, Levels, and Levels RMS measurement can also be used on NRZ waveforms (0 and 1 levels for one eye).

Most PAM toolbar measurements are compatible with PAM4, PAM6, and PAM8 waveforms. Some measurements support PAM4 only. PAM support is noted in each measurement's help topic.

PAM Measurements and Supported Waveforms
Measurement Waveform Types
NRZ PAM4 PAM6 PAM8
Ceq Noise Gain ● ●
CER Noise Margin (rms) ●
CER TDECQ ●
EECQ ●
Eye Heights ● ● ● ●
Eye Levels ● ● ● ●
Eye Skews ● ● ● ●
Eye Widths ● ● ● ●
Levels ● ● ● ●
Levels Peak-Peak ● ● ● ●
Levels RMS ● ● ● ●
Levels Skews ● ● ● ●
Linearity
RLM (802.3 CL_94) ● ● ● ●
RLM (802.3 A_120D) ● ●  
Eye Linearity (CEI) ● ● ● ●
Noise Margin (rms) ●
Outer Extinction Ratio ● ● ● ●
Outer OMA ● ● ● ●
PAM Overshoot ● ● ● ●
PAM Undershoot ● ● ● ●
Partial EECQ ●
Partial Noise Margin ●
Partial SER ●
Partial TDECQ ●
Pk-Pk Amplitude ● ● ● ●
Pmax ● ● ● ●
Pmin ● ● ● ●
TDECQ ●
Transition Time ● ● ●
Tx Power Excursion ● ● ● ●
Vertical Eye Closure ● ● ● ●