DDJ (p-p) Result
Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
NRZ
Package License:
L-RND
The Jitter mode Data Dependent jitter (DDJ) measurements is pattern-related jitter caused by the combined effects of Inter-Symbol Interference (ISI) and Duty Cycle Distortion (DCD). In Jitter Mode, Data Dependent Jitter is the peak-to-peak spread of the histogram of all edges as shown in the DDJ Histogram graph.
More Information
SCPI Command
:MEASure:JITTer:DDJ