UJ (rms) Result)

Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
NRZ
Package License:
L-RND

Click the Measurement (Meas) toolbar's UJ to activate Jitter mode's Uncorrelated Jitter (UJ) measurement which is the total of the following values:

  • Random Jitter (RJ) that is unpredictable and not data related, and
  • Asynchronous Periodic Jitter (APJ) that is periodic jitter that is uncorrelated to the symbol rate.

The relationship of UJ is shown in the Jitter Components Tree.

More Information

SCPI Command

:MEASure:JITTer:UJ