Measurement Levels Results
Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
NRZ
Package License:
L-RND
Measures the jitter sampling level, which is the amplitude at which jitter measurements are made. Jitter sampling level is specified as a percentage, custom, or average value in the Thresholds tab of the Jitter Mode Measurement Setup dialog. This measurement can only be viewed in the results table by sending the :MEASure:JITTer:LEVel command.
More Information
SCPI Command
:MEASure:JITTer:LEVel