Legacy External Application Licenses
This topics covers legacy FlexDCA applications for which the licensing was handled by FlexDCA and shown in the FlexDCA Licensing dialog. These applications have been replaced by new application versions. These new applications:
- Have new model numbers.
- Do not appear in the FlexDCA Licensing dialog.
- Are listed in the Keysight License Manager which is an application that is installed on the PC.
- Do not return an identifier response string from the remote
*OPT?query.
| Model Number | Description | *OPT?1 |
|---|---|---|
| N1012A-CEI | OIF CEI Compliance Application | CEI |
| N1014A-1FP | SFF-8431 Host Measurement Suite | HST |
| N1014A-2FP | SFF-8431 Module Measurement Suite | MOD |
| N1019A-UDA | User Defined Application | MYC |
| N1081A-1FP | IEEE 802.3ap/ba, Clauses 72,84 | IE1 |
| N1082A-1FP | IEEE 802.3ba, Clauses 83A,83B,86A | IE2 |
| N1082A-4FP | IEEE 802.3bm-2015 CAUI-4 Measurements | CA4 |
| N1083A-1FP | IEEE 802.3ba, Clause 85 | IE3 |
| N1084A-1FP | IEEE 802.3bj, Clauses 92,93 | IE4 |
| N1085A-1FP | IEEE 802.3bs Draft PAM4 Measurements | PM1 |
| N1085A-4FP | OIF-CEI 56G Draft PAM4 Measurements | PM4 |
| N1091BSCA | IEEE 802.3bs/cd Measurement Application | PM2 |
| N109256CA | OIF-CEI-56G-VSR/MR/LR Measurement Application | PM5 |
| N1091BSUA | IEEE 802.3bs/cd Measurement Application, N1085A Upgrade | PM2U |
| N109256UA | OIF-CEI-56G-VSR/MR/LR Measurement Application, N1085A Upgrade | PM5U |
| Footnotes: | ||
1. Characters that identify a feature in the string returned by the *OPT? common programming query. |
||
| Description | Model Number | OPT?1 |
|---|---|---|
| Advanced Eye Switch Control | 86100D-7FP | 40S |
| OIF CEI Compliance Switch Control | N1012A-7FP | CES |
| SFF-8431 Measurement Suite Switch Control | N1014A-7FP | SFS |
| User Defined Application Switch Control | N1019A-7FP | MYS |
| IEEE 802.3 Compliance Switch Control | N10812/3/4/5A-7FP | IES |
| PAM4 Switch Option for Ethernet and OIF-CEI App | N1085A-7FP | PMS |
| Footnotes: | ||
1. Characters that identify a feature in the string returned by the *OPT? common programming query. |
||