Licensed Features
The Licensed Features tab in the Licensing dialog shows Flex-series application features added by software package licenses listed in the dialog's Licenses tab. These features are not available on their own as a single license.

FlexDCA Package Licensed Features
This table shows all the available features for all FlexDCA license packages. The table also shows if a FlexDCA feature is shared with another license package and has active links to feature topics that are available in this help.
Characters that identify a feature in the string returned by the *OPT?
common programming query.