De-embedding Fixture Components
A Fixture Component models a test-setup component that has a non-connectorized port. Fixture Components are created in the Fixture De-embedding Setup pane of the TDR Setup dialog.
- For fixtures with a non-connectorized port:
- Click Launch AFR Wizard (
) to start FlexDCA's PLTS AFR. Or, - Drag an AFR Fixture Component symbol (
) to the Fixture De-embedding Setup diagram. This launches Quick AFR. Quick AFR characterizes the fixture, saves the Touchstone files, and automatically loads the Touchstone file into a new Fixture Component.
To create a new Fixture Component
Fixture Components represents a fixture that you want to de-embed. Up to 16 Fixture Components can be created and they are labeled "A" through "P". Once created, you drag a Fixture Component to the Fixture De-embedding Setup drawing that is located in the center of the dialog. You must characterize a fixture before you can create a Fixture Component. Characterization results in an S-parameter Touchstone file that is imported into the TDR Setup dialog to create a Fixture Component.
- If the Load From File button is not shown in the dialog's left-side panel, click the add new Fixture Component button.
- Make one of the following selections:
-
Click Load From File, and import the data from your Touchstone S-parameter file. This creates a new Fixture Component and labels it with the first available letter between "A" and "P". A total of 16 fixture components can be created. Or, -
Click the AFR symbol to start Quick AFR. Quick AFR is an abbreviated version of Full AFR that offers a smaller set of options and automatically loads the created Touchstone fixture characterization file into the new Fixture Component.
To de-embed an Fixture Component
- Select an existing Fixture Component.
- Click the Details button to identify how the port data within the S-parameter file is ordered. Because the port ordering method can vary depending on the S-parameter file, use this command to allow FlexDCA to correctly interpret the S-parameters.
- Drag your Fixture Component to the setup diagram.
- To reverse the ports on a Fixture Component, click the gear
icon. - Click Back to DUT layout to close the Fixture De-Embedding Setup.
| Fixture Component | Description |
|---|---|
|
Default port order.![]() |
|
Alternate port order.![]() |