:TPRogram:SLINe:CRPReset
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SLINe:CRPReset "<preset-name>"
Where <preset-name> is the name of a FlexOTO Clock Data Recovery (CDR) Preset.
Query Syntax
:TPRogram:SLINe:CRPReset?
Query Response
"<preset-name>"
For example, "IEEE 802.3bs/cd/ck (53 GBd)". Notice that the response includes double quotes.
Description
When editing an existing line in a Test Program, selects the Clock Data Recovery (CDR) Preset to be applied.
| CEI-112G-VSR/MR/LR (53 GBd) |
| CEI-56G-VSR/MR/LR (26 GBd) |
| IEEE 802.3bs/cd (26 GBd) PAM4 (Covers the IEEE 802.3cu clause) |
| IEEE 802.3bs/cd/ck (53 GBd) (Covers the IEEE 802.3cu clause) |