:TPRogram:SLINe:ERUNits

Flex Apps:
FlexOTO
FlexOTO Instance:
Stations

Command Syntax

:TPRogram:SETup:ERUNits {DECibel | PERCent | RATio}

Query Response

{DEC | PERC | RAT}

Description

For a Station's selected Test Program line, selects the measurement units for the Outer Extinction Ratio (ER) measurement. The units can be set to Decibel (DECibel), Percent (PERCent), or Ratio (RATio). The default selection is Decibel.

When adding new lines to a Test Program, use the :TPRogram:SETup:ERUNits command.

Measurements Affected by Configuration Settings (PAM4 Waveform)
Measurement Power Units Outer ER Units Linearity Definition Target Transition Target Hit Ratio
:TPRogram:SLINe:PUNits :TPRogram:SLINe:ERUNits :TPRogram:SLINe:LDEFinition :TPRogram:SLINe:TRANsition :TPRogram:SLINe:THRatio
Average Power ■
Ceq Noise Gain
Levels ■
Linearity ■
Outer ER ■
Outer OMA ■
Overshoot ■
Peak-Peak Power ■
TDECQ
Transition Time ■
Tx Power Excursion ■ ■
Undershoot ■