:TPRogram:SLINe:PUNits

Flex Apps:
FlexOTO
FlexOTO Instance:
Stations

Command Syntax

:TPRogram:SETup:PUNits {DBM | WATT}

Query Response

{DBM | WATT}

Description

For a Station's selected Test Program line, selects the power measurement units shown in the following table. The units can be set to dBM (DBM) or Watts (WATT). The default selection is Watts.

When adding new lines to a Test Program, use the :TPRogram:SETup:PUNits command.

Measurements Affected by Configuration Settings (PAM4 Waveform)
Measurement Power Units Outer ER Units Linearity Definition Target Transition Target Hit Ratio
:TPRogram:SLINe:PUNits :TPRogram:SLINe:ERUNits :TPRogram:SLINe:LDEFinition :TPRogram:SLINe:TRANsition :TPRogram:SLINe:THRatio
Average Power ■
Ceq Noise Gain
Levels ■
Linearity ■
Outer ER ■
Outer OMA ■
Overshoot ■
Peak-Peak Power ■
TDECQ
Transition Time ■
Tx Power Excursion ■ ■
Undershoot ■