:TPRogram:SETup:TMPReset
Flex Apps:
FlexOTO
FlexOTO Instance:
Stations
Command Syntax
:TPRogram:SETup:TMPReset "<TDECQ-meas-preset>"
Query Syntax
:TPRogram:SETup:TMPReset?
Query Response
"<TDECQ-meas-preset>"
For example, "IEEE 802.3cd". Notice that the response includes double quotes.
Description
When creating a Test Program for a Station, selects the TDECQ Measurement Preset to be applied to the currently selected fixtures and Lanes. To select the fixtures and lanes, use the :TPRogram:SETup:FIXTure and :TPRogram:SETup:FIXTure:LANE commands.
| IEEE 802.3bs |
| IEEE 802.3bs Amended |
| IEEE 802.3cd (Covers the IEEE 802.3cu clause) |
| IEEE 802.3db/D2.0 |
| Fiber Channel PI - 7 Rev 0.13 |