:JSOurce Subsystem

Flex Apps:
FlexPLL

Use the :JSOurce (Jitter Source) subsystem to configure FlexPLL's Source instrument's output clock or data signal. FlexPLL supports two Keysight sources. The :JSOurce commands correspond to the Channel Setup fields in the Source Setup dialog. To connect the Source to FlexPLL, use the commands in the :RSOurce subsystem.

For these parameters, always use the commands in FlexPLL's :JSOurce subsystem. Do not set these parameters by sending equivalent commands directly to the source instrument. These settings must be under FlexPLL's control.

Command Compatibility Vs. Source Instrument
Command Source Instrument
M8050A M8040A M8020A 81160A 81150A
:JSOurce:AMPLitude ■ ■ ■ ■ ■
:JSOurce:CHANnel ■ ■ ■ ■ ■
:JSOurce:CMODule ■    
:JSOurce:COUPling ■ ■ ■
:JSOurce:FORMat ■ ■ ■
:JSOurce:JPPeak ■ ■ ■ ■ ■
:JSOurce:MNUMber ■ ■ ■ ■ ■
:JSOurce:MODule ■ ■ ■
:JSOurce:MODule:MNUMber ■ ■ ■ ■ ■
:JSOurce:MODule:SNUMber ■ ■ ■ ■ ■
:JSOurce:OENable ■ ■ ■ ■ ■
:JSOurce:OFFSet ■ ■ ■ ■ ■
:JSOurce:PATTern ■ ■ ■
:JSOurce:RATE ■ ■ ■ ■ ■
:JSOurce:SCRate ■ ■ ■
:JSOurce:SNUMber ■ ■ ■ ■ ■
:JSOurce:WTYPe ■ ■ ■