:CHANnel:PROBe:ADAPter:ID?
Query Syntax
:CHANnelN:PROBe:ADAPter:ID?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
When a probe interface adapter is connected (see :CHANnel:PROBe:ADAPter:STATe?), this query returns the model number of the probe interface adapter.