:CHANnel:PROBe:VTValue

Command Syntax

:CHANnelN:PROBe:VTValue <voltage>

<voltage> is a double.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:PROBe:VTValue?

Description

When the INTernal voltage termination mode is selected (see :CHANnel:PROBe:VTMode), this command specifies the internal voltage termination value.