:CHANnel:PROBe:CORRection:MODE
Command Syntax
:CHANnelN:PROBe:CORRection:MODE {AUTomatic | REMove | OFF}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:PROBe:CORRection:MODE?
Description
Specifies the probe correction mode:
AUTomatic— When a probe contains an S-parameter description of its own electrical characteristics, as with InfiniiMax probe amplifiers, the oscilloscope will apply the proper correction for the probe. This is known as factory AC response calibration.REMove— Selects the Remove Probe/Cable correction mode. See :CHANnel Cable/Probe Remove Commands for a description of the commands that control these AC response calibrations.OFF— Automatic probe correction is off.