:CHANnel:PROBe:CAPacitance?

Query Syntax

:CHANnelN:PROBe:CAPacitance?

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

This query returns the capacitance of the probe.