:CHANnel:PROBe:UNITs

Command Syntax

:CHANnelN:PROBe:UNITs {AMPere | VOLT | WATT | UNKNown}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:PROBe:UNITs?

Description

Specifies the units for a probe.