:CHANnel:PROBe:ADAPter:STATe?

Query Syntax

:CHANnelN:PROBe:ADAPter:STATe?

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

The query returns a 0 (not connected) or 1 (connected) for probe interface adapter connection status.

For example, if the N2852A AutoProbe II to AutoProbe III interface adapter is connected to the channel, this query returns 1.

Query Response

{0 | 1}