:CHANnel:PROBe:ATTenuation

Command Syntax

:CHANnelN:PROBe:ATTenuation <attenuation>

<attenuation> is a double.

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:PROBe:ATTenuation?

Description

If the probe lets you set an attenuation/gain/dB value, you can use this command to set the value as an attenuation ratio (to 1).

The query returns the probe's attenuation/gain/dB setting as an attenuation ratio.

You can also specify a probe's attenuation/gain/dB setting using the :CHANnel:PROBe:GAIN or :CHANnel:PROBe:DB commands, respectively. These commands give you three ways of interpreting the same setting.