:CHANnel:PROBe:ID?
Query Syntax
:CHANnelN:PROBe:ID?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
Returns the model number of the connected probe or the "No Probe" string if no probe is attached to the channel input.
Use the :CHANnel:PROBe:STATe? query to see if any probe is currently connected.
Use the :CHANnel:PROBe:OMODe command to specify differential or single-ended measurements.