:CHANnel:PROBe:COUPling
Command Syntax
:CHANnelN:PROBe:COUPling {GND | DC | AC | ACLF1 | ACLF2 | ACLF3 | VC | OFF}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:PROBe:COUPling?
Description
Most Keysight probes are DC coupled, but if a probe has the options for different coupling, they will be available here.
Probe coupling mode is independent of any channel input coupling mode.