:CHANnel:COLor

Command Syntax

:CHANnelN:COLor  TCOLor{1:48}

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:COLor?

Description

Selects the color used to identify a channel on the screen. Waveform color assignments are saved as part of an instrument Setup file (:DISK:SETup:SAVE). Waveform colors are reset to their default values by a default setup (:SYSTem:DEFault) or factory default (:SYSTem:FACTory).

Channel Colors Versus Command Arguments
Color Argument Color Argument Color Argument Color Argument
TCOLor1 TCOLor2 TCOLor3 TCOLor4
TCOLor5 TCOLor6 TCOLor7 TCOLor8
TCOLor9 TCOLor10 TCOLor11 TCOLor12
TCOLor13 TCOLor14 TCOLor15 TCOLor16
TCOLor17 TCOLor18 TCOLor19 TCOLor20
TCOLor21 TCOLor22 TCOLor23 TCOLor24
TCOLor25 TCOLor26 TCOLor27 TCOLor28
TCOLor29 TCOLor30 TCOLor31 TCOLor32
TCOLor33 TCOLor34 TCOLor35 TCOLor36
TCOLor37 TCOLor38 TCOLor39 TCOLor40
TCOLor41 TCOLor42 TCOLor43 TCOLor44
TCOLor45 TCOLor46 TCOLor47 TCOLor48

To change the color of waveforms other than channels, use the following additional :COLor commands that are located in other subsystems:

Additional :COLor Commands
Command Description
:CMODe:COLor Sets color of common-mode waveforms.
:DIFF:COLor Sets color of differential waveforms.
:CGMemory:COLor Sets color of color grade memory waveforms
:FUNCtion:COLor Sets color of math function output waveforms.
:CHANnel:COLor Sets color of S-parameter waveforms.
:WMEMory:COLor Sets color of waveform memories.

Example Command Sequence

:CHANnel1_2:COLor TCOLor8