:TRIGger:QUALify:FOQualify

Command Syntax

:TRIGger:QUALify:FOQualify 

Description

This command will force one acquisition into the qualify trigger software post-processing system so you can see what signals look like when no qualified triggers are occurring. It is similar to the [Force] key for hardware triggers when the Sweep is set to Trig'd.

This command is the same as clicking the Force One Qualify button in the graphical user interface's Qualification setup tab.